|
|
|
This is a maintenance release containing several fixes to issues found in 1.7.3.
|
|
|
|
|
|
TabbedGroups
Moving a page to another leaf could cause a crash to occur and has been fixed.
Moving a page to another leaf could cause the pages to disappear and has been fixed.
AtLeastOneLeaf set to false in InitializeComponent method would not be honoured
and a leaf would be created and shown when the form is shown. This has been corrected.
ActiveLeaf is no longer persisted into InitializeComponent as it makes no sense to do so.TabControl
New property DragOverSelect added so that when dragging over the tab control it will cause
a change in tab page after a short delay when hovering over a tab page header. This can be turned off
if not required by setting the this property to false.
New method TabPageFromPoint added that takes a client based mouse position and returns the tab
page from that position. This matches against the tab page headers to find a match. Returns
null if no match can be found.Docking
Saving a configuration would often crash and especially when any of the content are in
the auto hidden state. This has been corrected and should never crash.
Changes to the content title or image will now be reflected immediately in the auto hidden
tab stubs that are visible at the edge of the docking area. Previously the text or images
were not updated until the content was un-autohidden.
|
|
|
|
|
|
Building the samples
Each sample has been written in C# and VB.NET, so you should navigate to the appropriate language
version contained below the Magic Library 1.7.4\Samples directory. Double click the solution file
found and you will be presented with the list of available samples. Righ click the sample application of interest and
select the "Set as StartUp Project" option. Now select the "Debug \ Start" menu option and the
projects will be automatically compiled and the selected sample started.Building the Magic source code
Navigate to the Magic Library 1.7.4\Source directory and you will find a Visual Studio .NET solution
called MagicLibrary. Double click this solution and you will be presented with a project that includes all
the source code for building an unsigned version of the Magic Library. The output will be placed by default in the
Magic Library 1.7.4\Bin directory and given the name MagicLocalLibrary.dll to distinguish it from the
official signed version that is in the same location and called MagicLibrary.dll.Using Magic in your own applications
Either create a new project or load the existing project of interest and right click the References folder.
The will present a dialog box with the .NET tab already selected. Navigate down the list of assemblies in
this tab until you find the Magic entry which should then be selected. Your project now has a reference to
the official signed build of Magic. When you decide to distribute your project you will need to also distribute
the signed assembly which is contained in the Magic Library 1.7.4\Bin directory and called MagicLibrary.dll.
It is recommended that you add the signed version into the GAC during your own installation process.
|
|
|
|
|
|
There is no license fee or royalty fee to be paid at any time for using the
Magic Library. You are however requested to acknowledge the use of the library
and provide a link to our home page www.dotnetmagic.com from the
About box of your application.
You may include the source code, modified source code, signed assembly or modified
built assembly within your own projects for either personal or commercial use but excluding
the restrictions outlined below.
The following restrictions apply to all parts of the library, including all source code, assemblies,
samples and documentation...- The above items cannot be sold as is, either individually or together.
- The above items cannot be modified and then sold as a library component, either
individually or together.
In other words, if you are using the library to enhance your project then you
are fine. If you are trying to gain commercically from the library itself rather
than using it to enhance your own work then you are prohibited from its use.
If in any doubt they please contact us at
license@dotnetmagic.com for a quick determination.
|
|
|
|