********************************************************************************************************
GLOBAL DRIVE CONTROL - version 4.14.1
********************************************************************************************************

Lenze 8200, 9300 and ECS inverters can be parameterized and controlled with this software.

These functions can only be obtained from the full version:
- short commissioning dialogs
- function block editor
- oscilloscope function

-------------------------------------------------------------------------------------------------------------------------------------------

CAUTION

The user is provided with the software at issued. All risks regarding quality and the results obtained by application of the software, remain with the user. The user must take correspondng safety measures to protect the system against maloperation.

We do not assume responsibility for directly or indirectly caused damage, e.g. profit losses, order losses or any other detriment.

-------------------------------------------------------------------------------------------------------------------------------------------

SYSTEM REQUIREMENTS

- MS Windows XP 32 Bit as of SP3, Windows 7*, Windows 8*
- IBM-compatible PC from Intel - Pentium-333 Prozessor
- At least 128 MB RAM
- 250 MB free hard disk capacity
- At least 1024 x 768 pixels Screen resolution with 256 displayable colours
- Mouse
- CD-ROM drive
- Free slots/interfaces according to the requirements of the individual fieldbus interface module

* minor restrictions, which are displayed during installation.
-------------------------------------------------------------------------------------------------------------------------------------------

OPTIONS for Setup.exe (batch mode installation)

/S /M=input.cfg	
Installation in batch mode with configuration file (dialogs of setup program are not visible)
e.g.:	setup.exe /S /M=input.cfg

For an example see file "input.cfg"

-------------------------------------------------------------------------------------------------------------------------------------------

COMMUNICATION INTERFACES

RS232 / LWL / system bus (CAN) /

RS485 	(only with intelligent interface converter, i.e. automatic detection of the data flow direction)

OPC interface (only for OPC servers which comply with the DRIVECOM specification, version 1.0)

Please observe the following information on the communication interface Optical Fibre:
For communication with the drive use the optical fibre and observe the following when there is more than one drive connected:
"Search all baud rates" may not be activated for the dialog "Lecom-A/B - Find drives"!

-------------------------------------------------------------------------------------------------------------------------------------------

DIRECTORY STRUCTURE

The individual components of GLOBAL DRIVE CONTROL are stored in different directories. The directory structure must not be changed.

\GDC
   |
   +-- \BIN
   |
   +-- \PDB 
   |
   +-- \DAT
   |
   +-- \DLL
   |
   +-- \HLP
   |
   +-- \OSZ
   |
   +-- \FBE

Contents of the directories:

\bin
Executable program file gdc.exe, program library and configuration files

\pdb
Directory for the storage of the unit descriptions required by GLOBAL DRIVE CONTROL. The file extension of these files is always *.pdb.
The unit descriptions are available in several languages. Therefore, the files are sorted according to the languages and saved in sub-directories. The identification code for the languages is identical to the language identification used in MS-DOS.

\dat
This directory saves the files with the parameter sets which are saved by the user. These files always have the extension *.gdc.

\dll
This directory contains drive-specific program libraries.

\hlp
Here you will find help files for the program GLOBAL DRIVE CONTROL as well as information about the inverters.

\osz
This directory contains the oscilloscope function

\fbe
This directory contains the function block editor

-------------------------------------------------------------------------------------------------------------------------------------------

SERIAL CONNECTION

The PC and the drive are connected via a cable with the following configuration:

  Lenze drive                                  PC
  9-pole SubD male plug  25-pole SubD female plug

  PIN                                   PIN
   2  o-------------------------------o  2
   3  o-------------------------------o  3
   5  o-------------------------------o  7


  Lenze drive                                  PC
  9-pole SubD male plug   9-pole SubD female plug

  PIN                                   PIN
   2  o-------------------------------o  3
   3  o-------------------------------o  2
   5  o-------------------------------o  5


All connections which are not listed, are not assigned. For further information see Operating Instructions Field-bus module type 2102 for RS232, RS485, optical fibre.

-------------------------------------------------------------------------------------------------------------------------------------------

TECHNICAL PROBLEMS

FAULT
Parameter-set file cannot be read

CAUSE-1
You tried to read in parameter-set files, which were generated by means of the DOS program 'Lemoc2' 

REMEDY-1
Global Drive Control uses a different format for filing the drive parameters. Transfer the parameter set from the controller to the PC and save it by means of Global Drive Control.

CAUSE-2
You tried to read in parameter-set files, which were generated by means of the test version (V0.6 ) of Global Drive Control program.

REMEDY-2
The type of the parameter-set file has changed from '*.VAR' to '*.GDC'. Please change the file type to '*.GDC' via the file manager.

FAULT
No controller communication.

CAUSE-1
You use a wrong PC-system cable.

REMEDY-1
Check system-cable wiring (see above)

CAUSE-2
Controller is switched off or no voltage applied to LECOM-A/B-module 2102.

REMEDY-2
Check voltage supply and controller connection. With external supply, check voltage  applied to terminals 39 and 59 (see corresponding Operating Instructions)

CAUSE-3
Wrong COM port selected

REMEDY-3
Set the used COM port under the menu  'Options/communication' of the Global Drive Control program.

CAUSE-4
Wrong setting of the interface parameter

REMEDY-4
The interface parameters can be changed thanks
to Windows system control:
-COM1: address 03F8, IRQ 4
-COM2: address 02F8, IRQ 3

CAUSE-5
Faulty Windows configuration.
The COM ports cannot be accessed via the Windows program 'Terminal'

REMEDY-5
Reinstall Windows or eliminate the fault in the configuration under the file 'System.ini'

-------------------------------------------------------------------------------------------------------------------------------------------

GDC with system bus driver:

NOTE
Files and entries in the SYSTEM.INI will not be deleted when GDC is uninstalled. 
Please ensure not using the Drive Developer Studio (DDS) when deleting the files and entries, otherwise DDS cannot communicate with the drive!

REMEDY-1 (Windows 9x)
Delete the following files:
\WINDOWS\SYSTEM\PEAKCANL.VXD
\WINDOWS\SYSTEM\VCANW32.DLL
oder
\WIN95\SYSTEM\PEAKCANL.VXD
\WIN95\SYSTEM\VCANW32.DLL

Delete the following entries (SYSTEM.INI):
device=peakcanl.vxd
[PEAKCAN]
Hardware1=2,0x378,7
Net1=GDC-PeakNet_1000, 1, 0x0014
Net2=GDC-PeakNet_125, 1, 0x031C
Net3=GDC-PeakNet_250, 1, 0x011C
Net4=GDC-PeakNet_50, 1, 0x472F
Net5=GDC-PeakNet_500, 1, 0x001C

REMEDY-2 (Windows NT 4.0)
Delete the following files:
\WINNT\SYSTEM32\DRIVERS\PEAKCAN.SYS
\WINNT\SYSTEM32\VCANW32.DLL

-------------------------------------------------------------------------------------------------------------------------------------------

SERVICE

If you have technical problems with GLOBAL DRIVE CONTROL, please contact your Lenze representative or our hotline.

Lenze Hotline 05154/82-1111